Part Number: DP83826I
Hello Experts,
My customer has question as follows. Would you answer it, please?
Q1. Suppose you are using basic mode and pulled down to Strap0(pin#16)=low. If the IC starts up in this state, is it OK to recognize that it will work in Full-Duplex without changing the BMCR bit8 (Duplex Mode) in SMI?
Q2. If device start up in Q1 condition, will the BMCR bit8 (Duplex Mode) follow Strap0 and enter "1"?
Q3. If you are using Strap2(pin#30) and Strap1(pin#31) in basic mode and are using Strap1(pin#31) in the default state. If SMI changes BMCR's bit12 (Auto-Negotiation Enable) and bit13 (Speed Selection) after the IC is started in this state, is it OK to recognize that it can be forced to operate in 10Base-T.
Q4. If a hardware reset (pin#32) or BMCR bit15(Reset) is performed, does the IC start up with the value set by the Strap pin after each register value has been reset?
Best Regards,
Fujiwara