Other Parts Discussed in Thread: ALP
************************
Hi
Our customer connect their own test card to the Deserializer EVB, which includes the ds90uh949 IC,
When the SER-DES lock is done with the UCD-323 pattern generator, we can get the LVDS output from the DES and read it in the internal EDID located in the IC. CASE-1
However, when we try it with HDMI, the PC does not see second screen, so we cannot get LVDS output, CASE-2
I share the data below via the ALP GUI of both halves, we are waiting for your return.
UCD-323: Pattern Generator used; CASE-1

PC HDMI Port used: CASE-2

-------------------------------------------------------------------------------------