Part Number: SN75179B
Other Parts Discussed in Thread: THVD1451, THVD1551, SN65HVD50, SN65HVD179, SN65LBC179A
Hi team,
Do we have new p2p pipeline for SN75179B? Customer has higher requirements for ESD rating and temperature range.
Nison
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75179B
Other Parts Discussed in Thread: THVD1451, THVD1551, SN65HVD50, SN65HVD179, SN65LBC179A
Hi team,
Do we have new p2p pipeline for SN75179B? Customer has higher requirements for ESD rating and temperature range.
Nison
Hi Nison,
The suggestions Clemens made are good options - this part is in a standard pinout so most other half duplex devices are pin compatible - but the THVD1551 and THVD1451 are good potential options .
What are the ESD requirements and temperature requirements of the customer system - while the two options are good options we may have a better one depending on customer need - so please let me know!
Best,
Parker Dodson
In this case, the only possible alternatives are the older SN65LBC179A, SN65HVD179, and SN65HVD50, which are more expensive and have a narrower temperature range and no better ESD.
Hi Clemens,
You firstly recommend THVD1551 and THVD1451 then you said "the only possible alternatives are the older SN65LBC179A, SN65HVD179, and SN65HVD50". Should I recommend THVD1551 to customer?
Nison,
The THVD1551 is p2p with SN75179B and the TI recommended upgrade.
The THVD1451 is possible - but the THVD1551 is the highest rec. upgrade for this device.
Best,
Parker Dodson
Sorry; I was unclear. Those three SN65xxx devices are alternatives to the THVDxxx devices.