Part Number: SN65DSI83
The LVDS output of the sensor is about 2.5Gbps bus bandwidth, the main control is Ti's ARM core board (MIPI's 4-lane CSI-2 interface), the resolution is 1280*1024, 200fps, from the LVDS output format on the sensor side to MIPI csi-2 format, and then connected to the MIPI CSI-2 interface on the ARM processor side,SN65DSI83 just csi to LVDS, is there this LVDS to MIPICSI-2 interface recommendation?