Part Number: TFP401
Other Parts Discussed in Thread: SN74LVC14A
I plan to use PanelLink Receiver in my design.
I chose TFP401 as a replacement for SiI1151[Silicon Image].
I have a few questions about designing the board.
I wasn't able to get a clear answer from the materials provided.
I would appreciate it if you could answer here.
1. When PDO#=LOW and in Output Drive Power Down Mode, is the state of the QE pin HIGH level, LOW level, or in an undefined state?
--- If it is in an undefined state, is it okay to connect a pull-down resistor to the QE pin? (To prevent malfunction of the input pin of the FPGA to which the QE pin is connected)
2. Is differential impedance control required for RX0+/-, RX1+/-, RX2+/-, RXC+/- traces?
--- If yes, what is the control value? Differential 50Ω?
3. What is the allowable trace length for output signals from the TFP401?
In the current situation where no measures are taken, it will be about 8 inches.
--- If I put a schmitt trigger (SN74LVC14A) in the output signal trace, is it right or wrong to put it in QE and ODCK?