Part Number: TUSB9261
Hi,
Recommended Operating Conditions for VBUS is max. 1.155V at datasheet. But, VBUS is suppplied by 5V at demo board.
Which one sould I use for VBUS in my design? => 1.1V (VDD) or 5V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB9261
Hi,
Recommended Operating Conditions for VBUS is max. 1.155V at datasheet. But, VBUS is suppplied by 5V at demo board.
Which one sould I use for VBUS in my design? => 1.1V (VDD) or 5V.
The VBUS pin must not be connected directly to the USB VBUS terminal.
The TUSB9261 has a threshold of about 0.5 V to detect that it is connected to a host. Use a voltage divider; see table 2 in section 8.2.1 for recommended resistor values.