Hello
Regarding DS90UB913Q-Q1 unused pin like: GPO_1,GPO2, GPO3,DIN10,DIN11 can be floating?
DS90UB914QSQ unused pin like: Rout10, Rout11, can be floating?
Roi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
Regarding DS90UB913Q-Q1 unused pin like: GPO_1,GPO2, GPO3,DIN10,DIN11 can be floating?
DS90UB914QSQ unused pin like: Rout10, Rout11, can be floating?
Roi
Hi Roi,
On the DS90UB913Q-Q1 GPO1, GPO3, DIN10, and DIN11 can be left floating. The GPO2 pin is recommended to be pulled to GND with a 40 kOhm resistor to ensure GPO2=LOW when PDB transitions from LOW to HIGH.
For the DS90UB914QSQ the unused pins Rout10 and Rout11 can be left floating.
Best,
Zoe