This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83TG720EVM-MC: Can not link DP83TG720-Q1 PHY to LAN8650 PHY 10 Mbit/s

Part Number: DP83TG720EVM-MC


Hi Ti experts,

I am using: DP83TG720 evaluation module for 1Gbps media converter; and connect this to LAN8650 PHY

The speed of DP83TG720 PHY as I know is 1Gbps and the speed of 

LAN8650 PHY is 10 Mbit/s.
I can not link up the connection between these 2 PHYs.

So my question is: the speed of 2 PHY must be the same => be able to link up 2 PHYs ?

And please give me some guide to link up 2 PHYs: setting,...

Thank you very much!

Dinh