Part Number: DP83867IR
For the PHY IC DP83867, when I do the strap configuration.
The datasheet shows that the default code of pin RX_CTRL is [00], which belongs to MODE1 and indicates enable the Auto-negotiation.
From datasheet, The MODE3 also enables the Auto-negotiation.
So, if I want to enable the Auto-negotiation, MODE1 and MODE3 are both OK, right?
But I found the strap configuration of RX_CTRL pin in TI demo board SK-64B_SCH is MODE3.
It confused me, why did they choose the MODE3 instead of MODE1?
Are there some other reasons?