This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9548A: Source series resistors?

Part Number: TCA9548A

Hello, I would like to ask if source series resistors are recommended on each of the SCn/SDn channels for signal integrity. If so, is there a recommended resistor value? Thanks!

  • This device is a passive switch; the SCn/SDn pins are not buffered. There should not be any series resistors.

  • Hey Jack,

    Is there a particular signal integrity issue that needs to be addressed? If the loading conditions on the I/Os are over the I2C standard (max of 400pF) then I2C buffers can be used in order to separate the capacitances from the I/Os. The I2C buffers can also be used to redrive the signals for cleaner signals as well. 

    Also see this app note for more information on buffers (page 8 and upwards).

    Regards,

    Jack