Part Number: TMUXHS4212
Hi
May I know TMUXHS4212 can be running 10gbps on A0p/n to B0p/n and B0p/n to A0p/n same channel?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMUXHS4212
Hi
May I know TMUXHS4212 can be running 10gbps on A0p/n to B0p/n and B0p/n to A0p/n same channel?
yes, it's bidirectional.
Regards
Brian
Hi Brian
1. If I use 10Gbase-T1, should I choose a, b, c block diagram application?
2. If the block diagram (c) is recommended, what voltage should be set for the pull-up Vbias?

Shawn
Hi brian
1.May I ask the full name of CM?
By the way 802.3ch vpp is 1.3v
2.If I use TMUXHS4212 in 10Gbase-T1 ,how many volts should VCC connect to?
Shawn
Shawn:
1: CM is common mode voltage.
2: 1.3v is single ended or differential, foe 4212, max differential voltage is 1.8v.
Regards
Brian