Part Number: SN55LVDS31
Other Parts Discussed in Thread: SN55LVDS32
Hi,
I can not seem to find the thermal resistance for the flat-pack package of the SN55LVDS31. I am looking for this one and the SN55LVDS32 flat-pack package as well.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN55LVDS31
Other Parts Discussed in Thread: SN55LVDS32
Hi,
I can not seem to find the thermal resistance for the flat-pack package of the SN55LVDS31. I am looking for this one and the SN55LVDS32 flat-pack package as well.
Hello Jacob,
Please see the thermal resistance for the SN55LVDS32 (W). I'm still working on the SN55LVDS31 package.
| Theta JA | 146.8°C/W |
| Theta JC (Top) | 80.2°C/W |
| Theta JB | 135.8°C/W |
| Psi JT |
57.3°C/W |
| Psi JB | 123.7°C/W |
| Theta JC (Bottom) | 14.2°C/W |
Regards,
Josh
Hello Jacob,
Please see the thermal resistance for the SN55LVDS31.
| Theta JA | 133.2ºC/W |
| Theta JC (Top) | 78.4ºC/W |
| Theta JB | 129.6ºC/W |
| Psi JT | 51.8ºC/W |
| Psi JB | 117.1ºC/W |
| Theta JC (Bottom) | 11.3ºC/W |
Regards,
Josh