Part Number: DS90UB941AS-Q1
I have a system with two separate 1440x1440 DSI outputs. So that's DS1 four lanes, DSI2 four lanes each showing a different picture.
At 60Hz that's a pixel clock of 124MHz, so can I only transmit one of these DSI busses per DS90UB941? Or can I transmit two (or maybe none). It wasn't clear to me after reading through the datasheet if dual mode meant I could run one DSI input up to 210MHz but then I needed two FPD Link outputs or if the only way to get to 210MHz was to have two DSI inputs running at 105MHz.
Thank you