Part Number: DS280DF810
Hi E2E Teams,
Maybe you can support me on this topic, my knowledge is based on reading and studying and I have limited hands on experience.
At this moment I am trying to find the best settings for DS280DF810 for 25.8 Gbs Ethernet connection.
Between the processor and the Retimer the atentuation is about 3.5dB at 12.9 Ghz. The same configuration is on the second board (the boards are identical). The boards are connected with a cable that has a atentuation of about 23dB at 12.9GHz. The cable connectors are QSFP+28.
Until now my results are:
Param(mode=2, maincur=22, precur=0, postcur=0, speed=100)
channel 0 - status: 0x30, heo: 0x0E, 0.438 UI, veo: 0x64, 312.5 mV
channel 1 - status: 0x30, heo: 0x10, 0.500 UI, veo: 0x5A, 281.2 mV
channel 2 - status: 0x30, heo: 0x10, 0.500 UI, veo: 0x5C, 287.5 mV
channel 3 - status: 0x30, heo: 0x0D, 0.406 UI, veo: 0x4E, 243.8 mV
channel 4 - status: 0x30, heo: 0x0F, 0.469 UI, veo: 0x5A, 281.2 mV
channel 5 - status: 0x30, heo: 0x0A, 0.312 UI, veo: 0x3E, 193.8 mV
channel 6 - status: 0x30, heo: 0x10, 0.500 UI, veo: 0x5A, 281.2 mV
channel 7 - status: 0x30, heo: 0x0D, 0.406 UI, veo: 0x3A, 181.2 mV
Even channels are TX, odd are Rx
Are these good values for HEO and VEO?
What can I do to improve the results? In which document can I find more info about the eye mask parameters for 100Gbs Ethernet?
Thanks in advance.