This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Customer looking for an Automotive Ethernet solution integrated with a vehicle computer.
The ideal solution would be a single chip that is compatible with 100/1000BASE-T1.
If you have a different recommendation, please feel free to let me know.
100Base-T1 Ethernet Transceiver
P83TC813R-Q1
1000Base-T1 Ethernet Transceiver
Micro TI DP83TG720R-Q1
Hi Gareth,
These recommendations can work. For the 100Base-T1 ethernet transmitter. You may also suggest the DP83TC814R-Q1 which is similar to the DP83TC812R-Q1, except it is slightly cheaper and does not offer TC10. Or you may also suggest the DP83TC813R-Q1 which is similar to the DP83TC812R-Q1 except it is smaller.
If you go on our product page, you can filter out devices based on the features you want: Ethernet PHYs product selection | TI.com
Best regards,
Melissa
Hi Gareth,
The DP83TG720S-Q1 is also an option, as it provides SGMII support in addition to RGMII support while the DP83TG720R-Q1 only provides RGMII support. Those are all your options.
Best regards,
Melissa