We develop an IoT gateway based on ESP32 + DP83848J as PHY for ehternet. The PHY is working properly getting the link when connected to a 100 Mbps switch. If we directly connect the Ethernet to a modem router (or some switches) it does not get the link. We produced 10 devices and not all of them show the same problem with the same network device (router/switches).
We made several tests and the strapping is OK, Voltages on PFB and RBIAS are OK.
Can someone give us some guidance how to proceed?
Thanks a lot