Part Number: TLIN1028-Q1
Hello,
I hope all is well.
Our design is using a 2u2 10% X7R 16V 0805 capacitor for Vcc signal at pin 8. Two devices are drawing current at around ~23 mA on the Vcc line not including the SBC internal logic current. Is this capacitor sufficient? Or is it recommend to use a 10 uF for this type of current draw.
Also, could you explain a little bit more in detail the difference between "Support no load to full load" and "20 uA to full load" from the TLIN1028-Q1 Automotive LIN 125-mA (SBC) datasheet.
Thanks and take care,