This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043G-Q1: Query about TCAN1043GDMTRQ1 wakeup times

Part Number: TCAN1043G-Q1
Other Parts Discussed in Thread: ISO7041-Q1, ISO1042, TCAN1043

Hello experts,

Regarding your company's TCAN1043GDMTRQ1, I would like to inquire about the following questions:

1. From a lifespan perspective, how many bus wakeup times can the transceiver support? (Transceiver wakes up through CAN/LIN bus)

2. Do transceivers have lifespan related parameter indicators?

3.What is the definition of common mode voltage in the datasheet? Vcom=(Vcanh+Vcanl)/2 ?

4.How to understand bus fault protection: ±58 V in the datasheet? Is there any connection between this parameter and the common mode voltage parameter?

5.Is there any connection between the ground offset of the transceiver and the common mode voltage parameters?

  • The second question is Do transceivers have lifespan related parameter indicators?

  • Wang,

    Thanks for your question and patience. We will have a response to you by end of business tomorrow CST.

    Regards,

    Eric Hackett

  • Hi Wang,

    For the first two questions, I have found a functional safety document on ti.com that describes different characteristics about the lifespan of the part here. I don't think we specifically conduct tests for your question 1, but the document might be of help.

    3.What is the definition of common mode voltage in the datasheet? Vcom=(Vcanh+Vcanl)/2 ?

    The equation that you describe here is the common voltage shared between the CANH signal and the CANL signal. This is the voltage that CANH and CANL will roughly settle at when in a recessive bit state.

    The common mode receiver voltage that you are pointing at in the datasheet is referring to the +/- 30V limit. This is generally saying that if there is a +/-30V ground shift in a system, the transceiver will still be able to operate correctly.

    4.How to understand bus fault protection: ±58 V in the datasheet? Is there any connection between this parameter and the common mode voltage parameter?

    The +/-58V bus fault protection refers to the maximum voltage that can be present on a single CAN line (either CANH or CANL), and describes the differential voltage that can be present on the CAN bus. You can find these limits in the abs. max conditions in the datasheet. These limits do vary between the version of the device you have. The "H" suffix can withstand up to +/-70V. 

    The common mode voltage parameter that you listed above where Vcom = (VcanH+VcanL) / 2 does not necessarily apply. The ground shifting however could. If the ground shift is large enough, this could potentially raise the potential on the CAN bus and put them close or over the +/-58V spec listed in the abs. max conditions. If the abs. max conditions are exceeded, there may be permanent damage to the device. 

    5.Is there any connection between the ground offset of the transceiver and the common mode voltage parameters?

    The ground offset of the transceiver would shift the common mode voltage parameter between CANH and CANL. For example, if your GND is shifted up 2V, you would expect CANH and CANL to both be shifting up 2V, which would shift the common mode voltage between them up 2V. Your differential voltage between CANH and CANL would not be affected because both CANH and CANL signals were equally shifted by the same voltage potential. 

    Regards,

    Tyler

  • Hello Tyler,

        Thanks for your detailed reply.

    For TCAN1043GDMTRQ1, common mode voltage is ±30V in normal mode and ±12V in sleep mode shown in the datasheet.

    1.Does this mean TCAN1043GDMTRQ1 can withstand ±30V GND shift in normal mode and ±12V GND shift  in sleep mode?

    2.If the max common mode voltage in our application is ±20V, both in normal mode and sleep mode:

    (1) What will happen in sleep mode if we use TCAN1043GDMTRQ1? Will TCAN1043GDMTRQ1 be damaged?

    (2)]From the perspective of cost and PCB space, we don't want to  add additional isolation devices(such as ISO7041-Q1) or use isolation CAN(such as ISO1042).  Base on above, what can we do to make TCAN1043GDMTRQ1 work normally in sleep mode in ±20V GND shift system?(such as  receiving wake-up signals Correctly  )

    Looking forward to your reply.

    Best regards!

    wang lei

  • Wang lei,

    1.Does this mean TCAN1043GDMTRQ1 can withstand ±30V GND shift in normal mode and ±12V GND shift  in sleep mode?

    The common mode voltage and GND shift are two separate but related characteristics. When the CAN bus is in a recessive state, the common mode voltage is roughly VCC / 2, or 2.5V. A ground shift could be present, say 2V for example. If the ground shift is 2V, this means that the common mode would be raised to 4.5V. 

    The +/-30V or +/-12V common mode spec is the maximum/minimum common mode voltage the receiver can withstand before operation of the device is compromised. A ground shift that would reach these limits would likely be slightly less than the common mode voltage produced by the transceiver. 

    (1) What will happen in sleep mode if we use TCAN1043GDMTRQ1? Will TCAN1043GDMTRQ1 be damaged?

    The TCAN1043GDMTRQ1 may only experience permanent damage if the absolute maximum conditions for the device are exceeded. Since you are experiencing +/-20V common mode voltage, this would not exceed the absolute maximum conditions. Since you are operating outside of the +/-12V during sleep mode, TI can no longer guarantee correct operation of the device, or the electrical characteristics listed in the datasheet, but the device would not experience permanent damage.

    (2)]From the perspective of cost and PCB space, we don't want to  add additional isolation devices(such as ISO7041-Q1) or use isolation CAN(such as ISO1042).  Base on above, what can we do to make TCAN1043GDMTRQ1 work normally in sleep mode in ±20V GND shift system?(such as  receiving wake-up signals Correctly  )

    TCAN1043 is spec'ed for +/12V common mode in sleep mode. There is no changing this parameter for this device, the changes will need to come from a system perspective. I recommend that GND loops would be minimized as much as possible in order to reduce any large ground potential differences in your system. 

    Regards,

    Tyler

  • TCAN1043 is spec'ed for +/12V common mode in sleep mode. There is no changing this parameter for this device, the changes will need to come from a system perspective. I recommend that GND loops would be minimized as much as possible in order to reduce any large ground potential differences in your system. 

    Hello Tyler,

        It's a good idea to minimize GND loops as much as possible.

    Is there any other way to improve the common mode voltage in sleep mode of TCAN1043?such as adding some electronic component in transceiver circuit?

    Below is our application. The right side(BMS in vehicle)is powered by 6V battery, the left side(DCDC charger) is powered by 26V DC power. The positive poles of the left and right are connected together while the negative poles are not connected together  because the low side switch is open. Under this condition, there will a 14V GND shift  between GND1 and GND2.

    In extreme cases, the ground offset will reach 20V in our application.

  • Wang Lei,

    There aren't really electrical components such as resistors, capacitors, chokes, etc. that would make a difference in the ground potential difference that is in your system.

    I recommend moving to some type of isolation at this point. It might be wise to look into an isolated CAN transceiver such as the ISO1042 in order to isolate this potential ground offset. 

    Regards,

    Tyler