Part Number: TRSF3221E
Hi,
I am considering using the TRSF3221E, but I need a short protection on its output.
The TRSF3221E typical short current is +/-35mA.
Is that mean I need to add series resistor of ~150ohm?
Or should I use additional protection IC.
If additional protection IC is needed, could you please advice me on one?
Additional question,
Do you have any mux or analog switch which can be fed by 3.3V or 5V for RS232 interface?
Thanks!
Erez.