Part Number: SN65HVD1040
Other Parts Discussed in Thread: TCAN334, SN74AHC1G125, TMS320F28377D
Is RXD/TXD pin supporting 3.3V level from MCU like as F28377?
Regards
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD1040
Other Parts Discussed in Thread: TCAN334, SN74AHC1G125, TMS320F28377D
Is RXD/TXD pin supporting 3.3V level from MCU like as F28377?
Regards
Brian
The TXD input can accept 3.3 V signals.
The RXD pin outputs 5 V; the TMS320F28377D will not work with this. You could insert a buffer with overvoltage-tolerant input (e.g., SN74AHC1G125), or use a 3.3 V CAN transceiver (e.g., TCAN334).
Brian,
Clemens is correct, please let us know any follow-up questions you may have.
Regards,
Eric Hackett