Part Number: DP83867IR
Hi Team,
According to datasheet 8.6.15 PHY Status Register (PHYSTS)
BIT NAME:WIRE_CROSS
Crossed Wire Indication:
Indicates channel polarity in 1000BASE-T linked status. Bits [5:2]
correspond to channels [D,C,B,A], respectively.
1 = Channel polarity is reversed.
0 = Channel polarity is normal.
However, is this polarity reversal function only for reversal detection?
Or is the polarity reversal processed and the data processed normally?
When connecting each channel to the connector, I reversed the P and M connections for each pair.
but it looks like auto-negotiation is completed.
Or is the polarity reversal processed and the data processed normally?
When connecting each channel to the connector, I reversed the P and M connections for each pair.
but it looks like auto-negotiation is completed.