Part Number: SN75LVCP600S
Other Parts Discussed in Thread: DS64BR111
The 600S is single-channel, and customer design requirements are dual-channel. So can customers use two 600S to design dual channels? We have also looked for other dual-channel ICs, but the temperature does not meet the requirements, the customer requires the operating temperature of -40 °C to 85 °C, and the current material of 600s meets the requirements. So customers want to know if the 600s can be used for dual-channel differential designs? The datasheet has a description of the dual-channel application, but does not detail the specific application and reference scheme of the dual-channel