Part Number: TCAN1044A-Q1
Hi team,
what's the ICC of each CAN in the following situation? thanks
when in the normal operation,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1044A-Q1
Hi team,
what's the ICC of each CAN in the following situation? thanks
when in the normal operation,

Hi Hazel,
In most cases, only one CAN transceiver will be driving a dominant state on the CAN bus at a time, so the dominant Icc will be the same as what is defined for the 60-ohm load case (70mA max). All other transceivers will be in a recessive state and therefore be consuming an Icc of 7.5mA max. Therefore, the average max draw of this system will be (70mA + 3x7.5mA) = 92.5mA.
Let me know if this is clear or if there is any part of your explanation that I am misunderstanding.
Regards,
Eric Schott