Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: ALP
Dear team,
We are using DS90UB960-Q1 forwarding stream sent by sensor with DS90UB953 serialiser. We only connect 1 sensor to DS90UB960 RX port 0.
I found that a multi-bit ECC error has been detected according to the value in register 0x4E(RX_PORT_STS2)=4d and 0x7A(CSI_RX_STS)=02 of DS90UB960.
This doesn't always happen, so we didn't store all the values in registers. But we can confirm that, when ECC_2_ERR is prompted in the deserialiser, the CSI data received by the serialiser has no errors, and the registers indicating CSI2 errors in the serialiser have no errors either.
My questions is: When ECC2_ERR detected by deserialiser,
1. What is the multi-bit ECC error meaning and why it only happend in deserialiser?
2. Is there any configuration set mistake in serialiser and deserialiser? Which part do we need to check?
3. Is this error indicating any mistake according to hardware working and design?
Any information may be helpful, thank you very much!