Please confirm that the DS100BR111 is more appropriate than the DS100BR111A for use with a 10GBASE-KR link (with link training on). We would also like to use the same part for a 1000BASE-KX link. I had noted that previous forum posts indicated that the only difference between the two parts was a 100mV shift in the VOD spec, but 10GBASE-KR compatibility seems like another major difference that was not previously disclosed.
If there is a better part for 1000BASE-KX, use please provide part number.
Thanks,
Mike