Part Number: TCA9543A
i would like to double confirm does it have repeater feature? thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9543A
i would like to double confirm does it have repeater feature? thanks.
there is a discreption on datasheet as Cb = total bus capacitance of one bus line in pF, does it mean could count capacitance separatly before TCA9543A and after TCA9543A.
No; all currently active bus segment are connected together and contribute to the bus capacitance.
Hello,
Clemens is correct. This device is a passive switch and does not buffer I2C signals (no repeating feature).
Cb = total bus capacitance spec'ed in the I2C standard. For standard mode or fast mode, the maximum parasitic bus capacitance that can be present on the bus is 400pF.
TCA9543A is not a true buffer, but it can separate bus capacitances by turning off channels of the device. However, as Clemens has already mentioned, every active channel of the TCA9543A connects to the I2C bus, and therefore contributes additional parasitic bus capacitance in parallel.
Regards,
Tyler
Hi Tyler,
So when the switch switch to channel 1, the total bus capacitance should calculate as :
Host side to the TCA9543A + TCA9543A second side channel capacitance + TCA9543A connect capacitance in sum ?
Thanks!
Kai
Hi Kai,
You are correct here!
Total cap would be = Host side cap + TCA9543A second side cap + any cap connected to the second side of TCA9543A (this includes trace cap + input capacitance for each slave device connected)
You can estimate cap as the following:
3 pF / inch of trace
~10pF input cap for each connected slave device unless otherwise specified in the datasheet.
Regards,
Tyler