Part Number: DS125DF1610
Hi expert,
According to table18 in DS125DF1610 datasheets, when 0x2F[7:4] is 0x7, the target rate supported are 12.5Gbps, 6.25Gbps and 3.125Gbps.
While in page41, the register map, 0x2F, "0x7: 12.5, 6.5, 3.125 Gbps", I think it might be a typo, can you help me to check that, 6.5Gbps is kind of strange.
Regards
Chris