Part Number: SN65LVDS3486
Other Parts Discussed in Thread: SN65HVD10, SN65HVD78, THVD1450
Dear Team,
I have a requirement in which I need to convert a LVTTL standard 1PPS(1Hz) signal of 50%,10%,1%,0.1% duty cycle to RS422 signal with lower skew(<3ns) and Higher slew rate(as good as possible).
Following part support the 1Hz signal and above mentioned requirements?
SN65LVDS3486D
If not Kindly suggest me the receiver part or transceiver part to use.