Part Number: DP83826E
Hello team,
I received 2 questions from the customer.
[Question 1]
The following statement is made on p. 45 of the data sheet,

Signal energy detect disable is recommended for EtherCAT. The customer assumes that the device is to be operated in RMII mode using Bootstrap, and Figure 9-11 shows that if RMII mode is selected, signal energy detect disable cannot be set. In this case, we will set "signal energy detect disable" in the PHY register setting after startup, but is the function the same as when "signal energy detect disable" is set in the Bootstrap above?

[Question 2]
This is a rudimentary question, but can you tell me why it is recommended for EtherCAT to disable signal energy detect for study purposes?
Regards,
Masa