This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042-Q1: CAN FD/XL Transceiver

Part Number: TCAN1042-Q1
Other Parts Discussed in Thread: TCAN6062, TCAN6062-Q1

Hi

could you help to suggest suitable products Thank you

CAN FD Transceiver : Bit rate Up to 8Mbit/s (5Mbit/s also available)

CAN XL Transceiver

  • Hi Gareth,

    The TCAN1044A (8-pin) or TCAN1043A (14-pin) would be my recommendations for a standard CAN FD transceiver that network support up the 8Mbps. If you are to be implementing CAN in a large or more complex network, you may be interested in upgrading to a CAN FD SIC transceiver with added ringing suppression such as the TCAN1462 or TCAN1463 (8- and 14-pin respectfully). 

    We are still developing our first CAN XL transceiver as the standard for this technology has not yet been fully released. The part number for this device will most likely be TCAN6062.

    Let me know if you have any more questions. 

    Regards, 
    Eric Schott 

  • Hi Gareth,

    Just following up here to let you know that the TCAN6062-Q1 and TCAN6062V-Q1 have been opened on ti.com for preproduction ordering.

    Best,

    Danny