This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: Queries regading DS90UB953-Q1 IC

Part Number: DS90UB953-Q1

Hi TI Team 

We are working with DS90UB953-Q1 IC and have some doubts - 

1.) We want to interface the output of the serializer directly to the serdes of the FPGA instead of using a cable and then using a deserializer IC as shown in the datasheet 

So on the FPGA side we have to decode the data because the IC is using encoder and then output is transmitted through cable driver. So can you please help us how to decode the data in the FPGA, so that we can use this IC in our application.  

2.) To drive the serial output of serializer TI is using a cable driver and we are connecting that output to a PCB trace of 100ohm and then to FPGA serdes through AC coupling. So will the IC support this configuration. 
  
3.) This IC supports 1 Gbps per lane of D PHY (4 Gbps for serial out), do TI have alternate IC that can operate on higher speed to support higher versions of MIPI DPHY like v2.0 

  • Hi,

    The FPD-Link encoding scheme is proprietary information which cannot be shared. You won't be able to use an FPD serializer without pairing it with a compatible deserializer.

    3.) This IC supports 1 Gbps per lane of D PHY (4 Gbps for serial out), do TI have alternate IC that can operate on higher speed to support higher versions of MIPI DPHY like v2.0 

    Yes we have faster devices but they are under NDA. I suggest reaching out to your local TI sales rep to inquire about these devices.

    Best,

    Lucas