This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP159: SLLA358

Part Number: SN75DP159
Other Parts Discussed in Thread: TDP142

Hi,

  We want to use X-MODE, do DP retimer, Can the code in SLLA358 be used?

  • Hi,

    Are you planning to use DP159 as a DP re-timer on the source or sink side?

    You can use the code in SLLA358 to configure DP159 as a DP re-timer on the sink side. But I would not recommend DP159 as a DP re-timer on the source side since its output is not designed to be DP compliant. For source side, please consider TDP142 or SN65DP141 re-driver.

    Thanks

    David