Part Number: TUSB320HI
Other Parts Discussed in Thread: TUSB320
Dears
Can you help review the SCH?
1. TUSB320 wants to implement as a Tpye-C, with CC1, CC2, and Rd pull-down when configured in DRP mode.Unable to discover and recognize Tpye-C devices at this time
2.Now using i2C mode high, I2C can scan to the address of 0x47, and then pull up 200k with the ID connected as devices. The port is suspended, the en enable pin is pulled up, the Rd connected to cc1 2 is 5.1k Ω to ground, and the pull up 200k Ω connected to out3 is 200k Ω. The values in registers 0x00 to 0x07 and spec match perfectly. Register 0x08 is 0x0c, register 0x09 is 0xf0, and register 0x0A is 0x00