Part Number: TUSB8020B
Other Parts Discussed in Thread: 3220UFP-DGLEVM, , HD3SS3220
Dear Sir or Madam, I am trying to connect a USB HUB to a USB-C port.
I purchased the 3220UFP-DGLEVM and connected it to an existing board with the TUSB8020B. Unfortunately, Windows cannot then find a HUB. I only need the USB3 part.
PC -> USB C -> HD3SS3220 -> TUSB8020
The lines for USB2.0 are not needed.
The TUSB8020 board works, without HD3SS3220, directly on a USB3.0 A port.
The Demo Board 3220UFP-DGLEVM also works when I connect a storage device directly.
But both in combination is not possible.
Both IC's should be on one board and powered only via USB.
Thanks for your help
with kind regards
M. Großmann