Part Number: TMUXHS4412
Other Parts Discussed in Thread: HD3SS3411, HD3SS3412, TMUX646
Hi team,
My customer want to find the high speed switch product whose requirements are as follows:
- Application: LCD test instrument, on high-speed video signals (differential), DP.
- Function: Choose one between signal source/open short circuit detection(2V 1mA) and screen, select the signal source to touch the screen, or select the open short circuit detection module to test the connection of the signal link.
- Rate: The current rate that needs to be supported is 8.1Gbps, 20Gbps products is developing, It is best for the product to be compatible with both rates (8.1Gbps/20Gbps)
Could you help recommend a suitable device that can support DP, DC supply(2V/1mA), 8.1GHz.
I recommended TMUXHS4412 before to use in DP(8.1GHz) and open/short circuit test(2V/1mA).
But it can not input 2V 1mA, right?
How to judge if the device can take 2V 1mA DC power.in input pin