Part Number: TCA9539-Q1
Other Parts Discussed in Thread: TCA9535, TS5A23157-Q1, TCA9548A-Q1, TCA6408A-Q1, TCAL9539-Q1,
Hi,
please suggest part with the same specifications & standards with having of 3 address bits
thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9539-Q1
Other Parts Discussed in Thread: TCA9535, TS5A23157-Q1, TCA9548A-Q1, TCA6408A-Q1, TCAL9539-Q1,
Hi,
please suggest part with the same specifications & standards with having of 3 address bits
thanks in advance
The TCA9535 replaces the reset input with a third address pin. But it does not have automotive qualification.
You could separate bus segments with an I²C switch like the TCA9548A-Q1 (8 channels) or a general-purpose switch like the TS5A23157-Q1 (requires a separate GPIO control signal).
TEMC,
Our only automotive grade 1 functional safety capable IO expanders are the TCAL9539-Q1, TCA6408A-Q1, and TCA9539-Q1. All of these devices have <3 address pins with the 6408A only having one address pin.
Clemens suggested a possible solution. There could be a separate bus segment with an I2C switch (TCA9548-Q1) or general purpose switch (TS5A23157-Q1) to help with lack of address pins. Of course the addition of these devices will require separate GPIO control signals.
Regards,
Tyler