Part Number: DP83867IS
Hi,
I am working on ethernet project on Xilinx Ultrascale+ which consists of the following:
TI dp83867is that is connected to AXI ethernet subsystem IP.
My design works at SGMII, 100Base-tx configuration.
in AXI ethernet subsystem I need to provide 125MHz clock mgt_clk that is routed from one of the quad transceivers.
From the PHY I have 625MHz differential clock [SGMII_COP,SGMII_CON]
is it possible to divide that clock to achieve 125mhz?
or do you have other suggestion for 125mhz from the PHY to Xilinx MAC?
I can add external differetial 125mhz clock to the the board, but if I have one in the PHY, I prefer to use it.