This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS171: I want to use the SWAP function of the TMDS 171.

Part Number: TMDS171

Hi,teams.

I want to use the SWAP function of the TMDS 171.

If I want to make the following connections, should I set the SWAP pin to High?

  • TMDS_clk- → IN_D2p(Port)
  • TMDS_clk+ → IN_D2n(Port)
  • TMDS_D0- → IN_D1p(Port)
  • TMDS_D0+ → IN_D1n(Port)
  • TMDS_D1- → IN_D0p(Port)
  • TMDS_D1+ → IN_D0n(Port)
  • TMDS_D2- → IN_CLKp(Port)
  • TMDS_D2+ → IN_CLKn(Port)

Thanks,

maru