Part Number: TUSB2046B
Other Parts Discussed in Thread: TUSB4020BI
Hi TI Guru,
I was overlooked the datasheet of USB hub, TUSB2046B and used it in my design that suppose need to support high-speed. Although the datasheet mention USB2.0, however, TUSB2046B only support 12Mbps which is USB1.1 speed.
Please recommended a replacement part that able to support 480Mbps.
If you could find a direct drop in would be very much appreciated.
If there are no any direct drop in for TUSB2046B, please recommend the part that meet below requirement.
1. USB2.0 480Mbps
2. Although TUSB2046B is 4 ports but our design just need 2 ports. Please recommended 2 ports part
3. We just use as a simple hub and do not need any monitoring etc.
Best regards,
Alder