Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD255: next gen

Part Number: SN65HVD255
Other Parts Discussed in Thread: TCAN1057A-Q1

Hi team, 

 Could you please kindly help provide next gen of SN65HVD255DR and related comparison table? it's better to be p2p. If no p2p, please provide the suitable device.  Thanks. 

BRs

Given

  • Hey Given,

    Please take a look at the TCAN1057A-Q1 for a direct P2P with the SN65HVD255DR. 

    Device: TCAN1057A-Q1 SN65HVD255DR 
    Protocols: CAN, CAN FD CAN 
    Supply Voltage:  4.5 to 5.5 4.5  to 5.5
    Bus Fault Voltage: -58 to 58 -27 to 40
    Max DR (Mbps): 8 1
    Rating Auto Catalog
    Low Power Mode: Silent Silent
    CMV: -12 to 12 -2 to 7

    Regards,

    Jack