Part Number: SN65DSI86
Hi TI,
We know the following parameters from Samsung's panel specification:
60Hz: VFP+VBP(with VS) (1848)
Can dsi86 support V Blanking=1848?
(We only use 60Hz)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Vertical Blanking=1848
Vertical front porch=8
Vertical sync width=8
Vertical back porch=1832
Horizontal Blanking=100
Horizontal front porch=32
Horizontal sync width=8
Horizontal back porch=60
frame=60Hz
RGB888
dual dsi
Width=2880
Height=1800
Please help confirm,Thanks!
Hi Chen,
DSI86 can only support data rates up to 5.4Gbps. It looks like this panel runs at 8.1Gbps, which the DSI86 cannot support.
Thanks, Allison
Hi Chen,
Typically, the eDP rate is fixed. We calculate the DSI rate by following the formulas in the DSI86 Programming Guide here: https://www.ti.com/lit/an/slla425/slla425.pdf
Given the above panel parameters, please note the below calculations:
Display pixel clock frequency = Htotal x Vtotal x refresh rate = 311MHz
Stream bit rate = pixel clock x 24bpp = 7GHz
Min required DSI clock frequency = stream bit rate / (2 x # of DSI lanes) = 460MHz (assuming 8 DSI lanes)
The DSI86 max DSI clock frequency is 750MHz. The DSI86 can support this panel as long as the refresh rate is 60Hz and the eDP speed does not exceed 5.4Gbps.
Thanks, Allison
Hi Allison,
For qualcomm platform, dual dsi means Width=1440 and lane=4 for a dsi.
pixel clock = Htotal x Vtotal x refresh = (1440+60+32+8)*(1800+1832+8+8)*60 = 337075200 , so pixel clock = 337MHz
bit clock = (Hactive + HBP + HFP + HSW) * (Vactive + VBP + VFP + VSW) * refresh * total bit per pixel / total lane num,
so, bit clock = (1440+60+32+8)*(1800+1832+8+8)*60*24/4=2022451200, bit clock = 2022.45MHz
dsi clock = bit clock / 2 = 1011.23MHz, one lane of a dsi was over 750MHz
My calculations are consistent with the qualcomm spreadsheet, and my calculations show that sn65dsi86 does not support this panel.
In the datasheet P48-P49, 0x36 is CHA_VERTICAL_BACK_PORCH(7:0), the max value of this register is 255, but the Vbp of the panel is 1832, over 255.
So the Vbp parameter off this panel is not supported?
Hi Chen,
Correct, the DSI86 will not support this panel if the DSI clock requires a frequency of 1011.23 MHz.
DSI86 cannot support a VBP of 1832 lines.
Thanks, Allison
Hi Chen,
The eDP data rate is typically fixed, and is given by the panel specification. DSI86 can support eDP data rates of 1.62 Gbps (RBR), 2.16 Gbps, 2.43 Gbps, 2.7 Gbps (HBR), 3.24 Gbps, 4.32 Gbps, or 5.4 Gbps (HBR2).
Are you asking about the stream bit rate? This can be calculated using the following formula: Stream Bit Rate = pixel clock x bpp.
Best, Allison