Other Parts Discussed in Thread: TPD4E02B04-Q1, TPD1E01B04-Q1
Hi Kenneth,
we are looking on how to do ESD protection of Rin+ and Rin- port when PoC is used.
you stated that the ESD diode should be place between the connector and the AC coupling capacitor. But later you suggested to look at app note slvaf60a where the diode is used between the Rin input and the AC coupling capacitor which is other way around from your first suggestion, please can you explain.
My understand is if PoC is used then we probably won't find a ESD diode with low capacitance and high Vrwm. Eg your suggested diode TPD4E02B04-Q1 has only 3.6 working voltage and if Poc is 5V,9V or 12V it won work.
Do you see any draw-back if using the ESD diode and a series resistor like in the slvaf60a app note? (TPD1E01B04-Q1 )
Are you aware of any layout that follows slvaf60a app-note, or did TI do any test with slvaf60a set-up?
Best Regards,
d.