This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi I have a similar request as descript in DS560MB410: Is DS560MB410 can be configured to support 1:2 fanout? - Interface forum - Interface - TI E2E support forums
But I'm mainly use in M-phy domain for the coming M-phy 6.0 which Bit rate will reach 39.936 Gbps with PAM4 modulation.
I have two questions here:
1. Does DS560MB410 have any AMI or Spice model for simulation?
2. Do DS560MB410 support M-phy? or any other can be used in M-phy?
Hi,
1) We do not have an IBIS-AMI model currently available, but we do have S parameters of the CTLE curves of this device. These can be found on mysecure. If you don't have access, you can request access with the link below.
https://www.ti.com/drr/opn/DS560MB410-DESIGN
2) Can you share any information on the M-phy electrical specification? In general, it sounds like 39.936 Gbps PAM4 is within the capabilities of the DS560MB410, but it would be helpful to reference the M-phy electrical specification to confirm.
Thanks,
Drew
Hi Drew:
Thanks for your reply.
You can access the M-phy 5.0 spec with the link below
And the current published version is 25G NRZ. The M-phy 6.0 for 39.936G PAM4 is still under investigating.
Hi,
Thanks for sharing. I will look into this further and get back to you this week.
Thanks,
Drew