Part Number: TLK6002
Hi
I am working with tlk6002 at 2.45Gbps data rate. I am using it for transmitting Video Data and doing External Loop-Back to see the received data on monitor.
The image is not reproducing correctly.Some of the video line data is missing.
There are no FIFO errors or ENCODE INVALID errors. But tlk6002 is giving DECODE INVALID error (THE REGISTER ADDRESS (0X05) VALUE IS 0X6103 ).
When I change the values in the register -0X02(CHANNEL_CONTROL_2) the image reproduction is changing.
In DEVICE INITIALISATION section(4.18) under 16-bit interface mode it is mentioned to choose the Values based on the desired application.

How to choose the values for register bits present in the above image?
Thanks & Regards
Mallikarjuna B