Part Number: DP83822I
Other Parts Discussed in Thread: TIDA-01463
We use the DP83822I in an POE application. During rapid disconnect/connect events of the ethernet cable, high voltages may occur on the PHY side of the magnetics in the PSE as well as in the PD.
As an ESD protection, a TVS diode TVS3V3L4U is placed between the magnetics and the PHY DP83822I.
Measurements on the TX and RX lines (pins 9, 10, 11, 12) still show voltages going below -1.0 V for > 200 ns, which is the lower limit listed in the absolute maximum ratings.
No destroyed parts have been reported so far, but the customer wants to be sure that there is no risk of damage for the DP83822I.
Looking at the ESD ratings for the pins affected, the device should be able to withstand voltages above or below the maximum ratings for a very short time. But the observed transients may well have longer durations compared to the ESD pulse specified in the IEC61000-4-2 standard.
Is additional protection needed? What is your suggestion on this issue?