Other Parts Discussed in Thread: TSB81BA3E
We are interfacing the TSB81BA3E D0-D7 data bus to an fpga running the LLC function. The TSB81BA3E is located about 3 inches away from the fpga and time domain reflectometry simulations indicate that unless the bus lines are terminated in the characteristic impedance of the lines, bad reflections will occur on the (100MHz) data bus and signal integrity will suffer. My question is whether the TSB81BA3E data bus lines (D0-D7) can drive 50 ohm terminated lines. The data sheet does not specify this. Thanks.