Part Number: MAX3237E
Hi,
Good Day.
I want to use the TI MAX3237ECDB as a drop-in replacement for an existing design.
The existing design has used the Maxim MAX3237CAI, ST Micro ST3237EBPR, and Intersil ICL3237ECAZ. All of these parts are pin-pin compatible.
I power the device with 3.3V and use 0.1uF ceramic X7R capacitors for the bypass and charge pump capacitors (C1-5 on your datasheet).
What I am concerned with is that your datasheet seems to indicate that 0.1uF caps will work for 3.3V ± 0.15V but suggests larger 0.22uF caps for 3.3V ± 0.3V.
While I believe my regulated supplies will hold a 5% tolerance, I am concerned that the other equivalent parts do not imply you need large caps for larger tolerances.
I want to be sure that the TI version is fully compatible with the other parts that only require 0.1uF caps.
Can you confirm that your part will work with 0.1uF caps even with a slightly larger than 5% power supply tolerance?
Please advise. Thank you very much.
Best Regards,
Ray Vincent