Part Number: TVP5150AM1
Other Parts Discussed in Thread: TVP5150, TVP5151
Hi team,
One of our customer's issues, could you please provide some troubleshooting suggestions
Basic status: Analog signal input to pin is normal, power supply is normal, crystal frequency is normal, and the polarity of DATA7 pin is inconsistent with DATA0~DATA6.
data2:

data7:

1. When using the following circuit, TVP5150 can be successfully configured by using I2C to set the 0X03 register to 0X6F, but the output image is incorrect and the input image is a color bar signal. What are the possible reasons for this phenomenon?
2. After removing the input capacitance of AIP1A, the analog signal is input, and there is an input waveform on the chip pins. However, when reading the 0XC0 register, it remains at 0x00. Is there a possible problem with the PCB design?

Input Test Image:

BT656 Port Output Image:

Best Regards,
Amy Luo