Part Number: TCA6416A
Other Parts Discussed in Thread: TCA6416, TCAL6416
Hi Team,
We would like to have the following startup sequence, Vcci, Vccp, Reset_high. It's noted in the DS that it is recommended Vccp should come up before Vcci, with the RESET being held low until both supplies are settled, do you see any potential issue or is the startup sequence valid?
Also, we will have I2C bus traffic talking to other devices while the TCA6416A will only have Vcci powered, (Vccp = 0V, Reset_LOW), is this possible or will the TCA6416 hold the bus low, or create a voltage divider preventing communication on the I2C bus?
Thank you,
Alex