Part Number: DP83848Q-Q1
I have a problem with DP83848QSQE circuit that is the low speed transfer of connection
I have checked the circuit and it seems that its fine, but for instance the scp command has the average speed of 60kb/s
following is the output of ethtool -S eth1:
NIC statistics:
Good Rx Frames: 1848
Broadcast Rx Frames: 15
Multicast Rx Frames: 116
Pause Rx Frames: 0
Rx CRC Errors: 8
Rx Align/Code Errors: 39
Oversize Rx Frames: 0
Rx Jabbers: 18
Undersize (Short) Rx Frames: 0
Rx Fragments: 0
Rx Octets: 2482973
Good Tx Frames: 1524
Broadcast Tx Frames: 96
Multicast Tx Frames: 52
Pause Tx Frames: 0
Deferred Tx Frames: 0
Collisions: 0
Single Collision Tx Frames: 0
Multiple Collision Tx Frames: 0
Excessive Collisions: 0
Late Collisions: 0
Tx Underrun: 0
Carrier Sense Errors: 0
Tx Octets: 131284
Rx + Tx 64 Octet Frames: 40
Rx + Tx 65-127 Octet Frames: 1506
Rx + Tx 128-255 Octet Frames: 147
Rx + Tx 256-511 Octet Frames: 28
Rx + Tx 512-1023 Octet Frames: 109
Rx + Tx 1024-Up Octet Frames: 1589
Net Octets: 2832168
Rx Start of Frame Overruns: 0
Rx Middle of Frame Overruns: 0
Rx DMA Overruns: 0
Rx DMA chan 0: head_enqueue: 1
Rx DMA chan 0: tail_enqueue: 1859
Rx DMA chan 0: pad_enqueue: 0
Rx DMA chan 0: misqueued: 0
Rx DMA chan 0: desc_alloc_fail: 0
Rx DMA chan 0: pad_alloc_fail: 0
Rx DMA chan 0: runt_receive_buf: 0
Rx DMA chan 0: runt_transmit_bu: 0
Rx DMA chan 0: empty_dequeue: 0
Rx DMA chan 0: busy_dequeue: 1650
Rx DMA chan 0: good_dequeue: 1732
Rx DMA chan 0: requeue: 0
Rx DMA chan 0: teardown_dequeue: 0
Tx DMA chan 0: head_enqueue: 1480
Tx DMA chan 0: tail_enqueue: 44
Tx DMA chan 0: pad_enqueue: 0
Tx DMA chan 0: misqueued: 44
Tx DMA chan 0: desc_alloc_fail: 0
Tx DMA chan 0: pad_alloc_fail: 0
Tx DMA chan 0: runt_receive_buf: 0
Tx DMA chan 0: runt_transmit_bu: 551
Tx DMA chan 0: empty_dequeue: 1480
Tx DMA chan 0: busy_dequeue: 0
Tx DMA chan 0: good_dequeue: 1524
Tx DMA chan 0: requeue: 0
Tx DMA chan 0: teardown_dequeue: 0